Hi
I'm using OMAPl138 processor and woking with Linux i need to implement UDP or TCP/IP programming is there any example for UDP or TCP/IP for OMAP-l138?
Thanks
Kumar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kumar,
You can find the ethernet driver details at the below wiki,
http://processors.wiki.ti.com/index.php/Building_03.22_PSP_release_Components_for_OMAP-L138#Ethernet
http://processors.wiki.ti.com/index.php/DaVinci_PSP_03.20.00.14_Device_Driver_Features_and_Performance_Guide#Ethernet_Driver
In addition that please check with linux psp for UDP/TCP test code.
I recommend you find the UDP send and receive test code at the NDK package.