This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515 spi EEPROM boot

Other Parts Discussed in Thread: TMS320C5515

Dear all;
I have a question about eeprom boot of TMS320C5515. Bootloader application note says that to boot from an spi eeprom,you should connect the CS of the eeprom to CS0 of DSP.I am a bit confused here because TMS320C5515 has 2  SPI_CS0 connections which can be selected using different EBSR  PPMODE  :one of them locates  at P4 (LCD_CS0_E0/SPI_CS0) other locates at P11 (LCD_D[9]/I2S2_FS/GP[19]/ SPI_CS0). Which one of them is selected by DSP during booting process? Is both of them selected consecutively one another? 

Regards