This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 Input current



Hi,

The datasheet shows the input current to be positive (+310uA) with internal pull-up resistor and negative (-270uA) with pull-down resistor. Is this a typo? Shouldn't the input current be negative when there is an internal pull-up resistor?

Thanks.

  • Hi John,

    The Negative value is given only for Pull-down conditions and not for the Pull-up condition.

    Regards

    Antony

    • --------------------------------------------------------------------------------------------------------
      Please click the Verify Answer button on this post if it answers your question.
      --------------------------------------------------------------------------------------------------------