We try to use 17 video decoder channels in DVRRDK 03.00.00.00, 16 channels are used for IP-camera decoding, 1 extra channel should be used for video playback. (All in 720x576) Currently we initialize 16 decoder channels. 15 channels are used for IP-camera decoding only and one decoder channels is shared between IP-camera and video playback. This works file. Now we want to use IP-camera decoding for 16 channels and video playback at the same time. If I setup maximal 17 decoder channels the system hangs at startup. (I have attache a log witch comment) As I understand it is possible to setup max. 64 decoder channels.
Next step will be to have 16 decoder channels for 720x576 for IP-camera and 1 decoder channel 1920x1080 for playback. But first we want to run all in 720x576 max.