can i use up to 1TB of ddr3 memory (LPAE) in OMAP 5?
And the memory controller, is it flexible? Can i change the parameters (ras, cas, etc)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
can i use up to 1TB of ddr3 memory (LPAE) in OMAP 5?
And the memory controller, is it flexible? Can i change the parameters (ras, cas, etc)?
Hello,
The Cortex A15 itself supports the LPAE.
But you can connect to the EMIF memory with up to 2GB density per chip select providing a total SDRAM space of 8GB addressable by the MPU extended address range.
You cannot connect 1TB of DDR3 directly to omap device.
Best Regards,
Yordan