This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does SYS/BIOS support new TMS320F28377D processor, and if not when?

Other Parts Discussed in Thread: TMS320F28377D

I just recieved the new F28377D control card and would like to start developing for this chip using either DSP/BIOS or SYS/BIOS. 

I have a large amount of code developed for the F28335 processor and with it I use DSP/BIOS (version 5.42.01.09).  Do you know if there is any chance someone will be creating a default DSP/BIOS config file for the controlF28377D? 

If not do you know when (if not already) will SYS/BIOS support the F28377D?  I am using CCS 5.5 and tried to build an example SYS/BIOS project for the F28377D that I found using the "resource Explorer".  It gives me a build error that "no target named" in the cmdr.xs file. 

The release notes for SYS/BIOS also do not state that the F28377D is supported. 

 

Thanks for the help

Dan