Hello. I have been creating a better OMAP3530 CBB symbol than the one currently supplied by TI and I have noticed that not all of the PoP balls show connections to bottom balls. Are these balls no-connects even though some of them are power balls? For example, PoP A4 (Vdd), B4 (Vss), C23 (Vddq), etc., do not show any feed-through to bottom pins of the CBB part. I do see these pins listed in the Table 2-25 of the datasheet (SPRS507F) and that they are connected somehow to power rails but I do not understand how they are attached to these power rails. Other power pins of the PoP are feed-throughs to bottom pins (e.g., PoP H22 (Vss), H23 (Vdd), L1 (Vcc), etc., which need to be connected to the appropriate power rail. Please clarify.
Regards,
Charles