Hello,
I'm using the DM8148 SoC and running it under OPP166 (ARM running at 1 GHz and DSP running at 750 MHz).
I'm trying to use QDMA channels 2 and 3 on the DSP side using the EDMA3LLD driver (version 02.11.05.02) to copy data from / to DDR and the LL2.
No changes were made to the ARM / Linux code regarding the EDMA init / usage and it's based on TI EZSDK v5.05.02.00.
The EDMA configuration on the DSP side is as follows: configuring it as master on EDMA region 1 and initializing the DMA / QDMA channels, TCCs and PaRAM sets association based on the table below (taken from the following link: http://processors.wiki.ti.com/index.php/TI81XX_PSP_EDMA_Driver_User_Guide):
Present configuration of EDMA3 resources on DM814X platform:
| EDMA3 Resource | DM814X | |
|---|---|---|
| ARM | DSP | |
| DMA Channel | 2-13, 16-25, 32-47, 52-55 | 0-1, 14-15, 26-31, 48-51, 56-63 |
| QDMA Channel | 0,1 | 2-7 |
| TCC | 2-13, 16-25, 32-47, 52-55 | 0-1, 14-15, 26-31, 48-51, 56-63 |
| PaRAM Set | 2-13, 16-25, 32-47, 52-55, 64-127 | 0-1, 14-15, 26-31, 48-51, 56-63, 128-511 |
My problem is as follows: after running the system, I'm able to see the QDMA transfers taking place. However, after a random period of time (usually a few seconds), the DSP is reaching an infinite loop (in my code) which polls the IPR register for the proper event (based on the last transfer).
Looking at the last PaRAM set associated with the last transfer, I saw that the transfer took place, but the transfer complete interrupt isn't set in the IPR for the transfer configured TCC).
I wasn't able to re-create the problem if I put breakpoints before initiating a transfer and before polling the IPR. Everytime I hit the pooling breakpiont, I could see the correct bit set in the IPR and the DSP continued its run.
What could be the cause for this problem? Could it be some sort of race condition between the ARM and the DSP?
Thanks in advance,
Elad.