This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use the TI-RTOS GUI for modular code generation on the c28

Hello,

I would like to know, if it was possible to use the GUI of TI-RTOS on the c28 for modular code generation on the c28 without having an OS on it. I have different ISRs in my file, which depending on the type of maschine i am in contact with(motor or generator for example)  should be processed. I was thinking about using the XDC Tools with Make, which is in XDC to generate an Executable but it would be great it it was possible to use the GUI of TI-RTOS to generate a file like config.cfg, which would help to create an Executable at the End. I would be thankful if you could give me some hints to solve my problem.

Joel