This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

why vote threshold is 15 in Table 9 ?

I have readed the <<SerDes Implementation Guide for KeyStone I Devices>>, it said twelve data bits constitute the

voting window. The twelve votes  are then summed, and an action to adjust the position of the sampling clock occurs

if  the difference between early and late vote s exceeds a programmable threshold.

But the max  vote threshold is 15 in Table 9 !


I was confused  why the threshold greater than twelve ?  In any case , there are twelve votes in a voting window.
Thank you !