This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Board Booting Issue (using OMAP4460 Jorjin ATCN module )

Hi All,

 we are designing custom board using Jorjin ATCN  module. we are working on Linux driver development.

looking for suitable file system.

we tried with both ubuntu FS and Blaze rootfs. board is not coming till the prompt.


Also we tried with Arago based rootfs which was working on AM3730  based Panther board.

with this board is coming till prompt. we are able enter commands like ls, ifconfig 

But some time during booting at  login itself it gives some junk and boot up hangs. below is the bootlog for your reference.

Note:  we are using arm tool chain(arm-2010q1) to compile kernel

Pls advise on this.

Thanks in advance.

Regards,

Raghunath 

Texas Instruments Inc X-Loader 1.41.0-gef79b791-dirty (Jul 10 2013 - 10:27:37)
OMAP4460: 1.2 GHz capable SOM
Starting OS Bootloader from MMC/SD1 ...


U-Boot 1.1.4-ge6f499d3-dirty (Jul 10 2013 - 10:26:59)

Load address: 0x80e80000
DRAM:  1024 MB
Flash:  0 kB
Using default environment

In:    serial
Out:   serial
Err:   serial
Battery not detected
Initializing SD(0) Slot.
ptbl slot: SD:(0).
efi partition table not found
efi partition table:
ptbl slot: EMMC:(1).
efi partition table not found
Net:   KS8851SNL
Hit any key to stop autoboot:  0 
Usage:
MMC sub system


5145944 bytes read
## Booting image at 81c00000 ...
   Image Name:   Linux-3.4.34
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    5145880 Bytes =  4.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK
I2C read: I/O error

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0
[    0.000000] Linux version 3.4.34 (udupitech@udupitech-desktop) (gcc version 4.4.1 (Sourcery G++ Lite 2010q1-202) ) #9 SMP PREEMPT Mon Jan 27 18:48:55 IST 2014
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: OMAP44XX Tablet board
[    0.000000] android_display: setting lcd resolution to 1280*800, bpp=4
[    0.000000] android_display: tiler1d 33554432
[    0.000000] android_display: setting fb0.vram to 4096000
[    0.000000] android_display: setting hdmi resolution to 1280*800, bpp=4
[    0.000000] android_display: tiler1d 33554432
[    0.000000] android_display: setting fb1.vram to 8192000
[    0.000000] android_display: setting vram to 12288000
[    0.000000] Cannot detect omap type!
[    0.000000] Reserving 12582912 bytes SDRAM for VRAM
[    0.000000] cma: CMA: reserved 16 MiB at ad800000
[    0.000000] Memory policy: ECC disabled, Data cache writealloc
[    0.000000] OMAP4: Map 0xaea00000 to 0xfe600000 for dram barrier
[    0.000000] OMAP4460 ES1.1
[    0.000000] PERCPU: Embedded 9 pages/cpu @c1293000 s12992 r8192 d15680 u36864
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 171264
[    0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait console=ttyO2,115200n8 root=/dev/mmcblk1p2 rw rootdelay=2 init=/init no_console_suspend
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 400MB 2MB 200MB 75MB = 677MB total
[    0.000000] Memory: 656944k/656944k available, 391632k reserved, 76800K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc091c000   (9296 kB)
[    0.000000]       .init : 0xc091c000 - 0xc09742c0   ( 353 kB)
[    0.000000]       .data : 0xc0976000 - 0xc0a13430   ( 630 kB)
[    0.000000]        .bss : 0xc0a13454 - 0xc0a89b38   ( 474 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] NR_IRQS:626
[    0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000183] Calibrating delay loop... 1392.74 BogoMIPS (lpj=5439488)
[    0.070343] pid_max: default: 32768 minimum: 301
[    0.070526] Security Framework initialized
[    0.070648] Mount-cache hash table entries: 512
[    0.071685] Initializing cgroup subsys debug
[    0.071716] Initializing cgroup subsys cpuacct
[    0.071716] Initializing cgroup subsys freezer
[    0.071746] Initializing cgroup subsys net_cls
[    0.071777] CPU: Testing write buffer coherency: ok
[    0.072021] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.072235] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.072357] Setting up static identity map for 0x806e77e0 - 0x806e7838
[    0.072387] L310 cache controller enabled
[    0.072418] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x7e470000, Cache size: 1048576 B
[    0.072906] generating sar_ram layout...
[    0.073089] sar ram layout created
[    0.150756] CPU1: Booted secondary processor
[    0.220703] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.220733] CPU1: Unknown IPI message 0x1
[    0.220764] Brought up 2 CPUs
[    0.220764] SMP: Total of 2 processors activated (2792.83 BogoMIPS).
[    0.224884] In Serial early init: uart1
[    0.224914] Udupitech: Early init of port ttyO0 0
[    0.224914] In Serial early init: uart2
[    0.224945] Udupitech: Early init of port ttyO1 1
[    0.224945] In Serial early init: uart3
[    0.224945] Udupitech: Early init of port ttyO2 2
[    0.224975] ttyO2uart is for console display
[    0.224975] In Serial early init: uart4
[    0.224975] Udupitech: Early init of port ttyO3 3
[    0.225006] In Serial early init: uart5
[    0.225006] In Serial early init: uart6
[    0.225006] In Serial early init: uart7
[    0.225036] In Serial early init: uart8
[    0.225036] In Serial early init: uart9
[    0.225036] In Serial early init: uart10
[    0.225067] In Serial early init: uart11
[    0.225067] In Serial early init: uart12
[    0.225067] In Serial early init: uart13
[    0.225097] In Serial early init: uart14
[    0.225097] In Serial early init: uart15
[    0.225128] In Serial early init: uart16
[    0.229156] omap_hwmod: aess: _wait_target_disable failed
[    0.231964] omap_hwmod: dss_dispc: cannot be enabled (3)
[    0.234680] omap_hwmod: dss_dsi1: cannot be enabled (3)
[    0.237396] omap_hwmod: dss_dsi2: cannot be enabled (3)
[    0.240112] omap_hwmod: dss_hdmi: cannot be enabled (3)
[    0.242828] omap_hwmod: dss_rfbi: cannot be enabled (3)
[    0.245574] omap_hwmod: dss_venc: cannot be enabled (3)
[    0.249389] omap_hwmod: mcpdm: cannot be enabled (3)
[    0.251220] omap_device: cannot add global notifier for dev PM QoS
[    0.251800] dummy: 
[    0.252838] NET: Registered protocol family 16
[    0.270019] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.270416] GPMC revision 6.0
[    0.272125] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[    0.272186] OMAP GPIO hardware version 0.1
[    0.272338] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[    0.272552] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[    0.272735] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[    0.272949] gpiochip_add: registered GPIOs 128 to 159 on device: gpio
[    0.273132] gpiochip_add: registered GPIOs 160 to 191 on device: gpio
[    0.274230] omap_mux_init: Add partition: #1: core, flags: 2
[    0.275115] omap_mux_init: Add partition: #2: wkup, flags: 2
[    0.277252] Udupitech: initialized HUB reset for USB-Ethernet 
[    0.282073] dmm dmm: initialized all PAT entries
[    0.283721] omap_mux_get_by_name: Could not find signal csi22_dx2.csi22_dx2
[    0.283752] omap_mux_get_by_name: Could not find signal csi22_dy2.csi22_dy2
[    0.284118] Udupitech: done with board initialization!!! 
[    0.284179] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.284179] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.287231] gcxxx_int failed. gcx hardware is not present
[    0.287414] OMAP DMA hardware revision 0.0
[    0.287963] emif emif.1: emif_probe: device configured with addr = f018a000 and IRQ142
[    0.288208] emif emif.2: emif_probe: device configured with addr = f018c000 and IRQ143
[    0.289337] SmartReflex Recalibration delay = 86400000ms
[    0.289367] SmartReflex Class 1.5 initialized
[    0.289703] Reprogramming LPDDR2 timings to 800000000 Hz
[    0.297637] bio: create slab <bio-0> at 0
[    0.298278] VBAT: 3750 mV 
[    0.298492] vwl1271: 1800 mV 
[    0.299499] SCSI subsystem initialized
[    0.299804] usbcore: registered new interface driver usbfs
[    0.299926] usbcore: registered new interface driver hub
[    0.300048] usbcore: registered new device driver usb
[    0.300964] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 400 kHz
[    0.302001] twl_core: detected twl6032 rev.1 eepromrev.56
[    0.303253] twl 1-0048: PIH (irq 39) chaining IRQs 416..436
[    0.304260] LDOUSB: 3300 mV normal standby
[    0.307891] twl6030_usb twl6030_usb: Initialized TWL6030 USB module
[    0.308807] VANA: 2100 mV normal standby
[    0.309509] CLK32KAUDIO: 
[    0.310455] SYSEN: 
[    0.311431] REGEN1: 
[    0.312103] CLK32KG: 
[    0.312408] V2V1: 2100 mV normal 
[    0.312438] V2V1: supplied by SYSEN
[    0.313110] LDO5: 1200 <--> 3000 mV at 3000 mV normal standby
[    0.314025] LDO1: 1800 <--> 2500 mV at 1900 mV normal standby
[    0.314941] LDO7: 1200 <--> 2900 mV at 1800 mV normal standby
[    0.316101] LDO6: 1800 mV normal standby
[    0.316314] LDO6: supplied by V2V1
[    0.317596] LDOLN: 1800 mV normal standby
[    0.317810] LDOLN: supplied by V2V1
[    0.318756] LDO2: 1000 <--> 3000 mV at 2800 mV normal standby
[    0.319671] LDO4: 1200 <--> 2800 mV at 1800 mV normal standby
[    0.320587] LDO3: 1000 <--> 3000 mV at 1200 mV normal standby
[    0.321838] SMPS4: 1800 mV normal standby
[    0.322235] twl6030: set (mod=0x0D reg=0x53 val=0x01): VCORE1 OFF=OFF SLEEP=OFF ACT=AUTO
[    0.322387] twl6030: set (mod=0x0D reg=0x59 val=0x01): VCORE2 OFF=OFF SLEEP=OFF ACT=AUTO
[    0.322509] twl6030: set (mod=0x0D reg=0xf6 val=0x77): VCORE1 disable PD on shutdown
[    0.322631] twl6030: set (mod=0x0D reg=0x5e val=0x00): VCORE3 - remove binding to groups
[    0.322753] twl6030: set (mod=0x0D reg=0x64 val=0x00): VMEM - remove binding to groups
[    0.323181] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 400 kHz
[    0.323577] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 400 kHz
[    0.323852] omap_i2c omap_i2c.4: bus 4 rev2.4.0 at 400 kHz
[    0.324127] Linux video capture interface: v2.00
[    0.324188] sr_init: No PMIC hook to init smartreflex
[    0.324707] omap-iommu omap-iommu.0: dsp registered
[    0.324798] omap-iommu omap-iommu.1: ipu registered
[    0.325042] Advanced Linux Sound Architecture Driver Version 1.0.25.
[    0.325744] Bluetooth: Core ver 2.16
[    0.325775] NET: Registered protocol family 31
[    0.325805] Bluetooth: HCI device and connection manager initialized
[    0.325805] Bluetooth: HCI socket layer initialized
[    0.325836] Bluetooth: L2CAP socket layer initialized
[    0.325866] Bluetooth: SCO socket layer initialized
[    0.327453] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[    0.327941] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[    0.328430] smartreflex smartreflex.2: omap_sr_probe: SmartReflex driver initialized
[    0.328460] Power Management for TI OMAP4XX/OMAP5XXX devices.
[    0.328796] omap_opp_set_min_rate: Missing opp info for hwmod hsi
[    0.328826] Forcing clock hsi_fck to minimum rate 96000000
[    0.328857] omap_opp_set_min_rate: Missing opp info for hwmod dsp_c0
[    0.328857] Forcing clock virt_dpll_dsp_ck to minimum rate 232750000
[    0.328918] omap_opp_set_min_rate: Missing opp info for hwmod aess
[    0.328918] Forcing clock abe_clk to minimum rate 98304000
[    0.329467] Switching to clocksource 32k_counter
[    0.349548] NET: Registered protocol family 2
[    0.349822] IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.350524] TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
[    0.352661] TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
[    0.353912] TCP: Hash tables configured (established 131072 bind 65536)
[    0.353912] TCP: reno registered
[    0.353942] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.353973] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.354309] NET: Registered protocol family 1
[    0.354705] RPC: Registered named UNIX socket transport module.
[    0.354736] RPC: Registered udp transport module.
[    0.354736] RPC: Registered tcp transport module.
[    0.354736] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.354888] usbhs_omap usbhs_omap: ehci_logic_fck failed:-2
[    0.356018] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.356781]  omap-rproc.1: alias fck already exists
[    0.376617] sr_classp5_calib_work: smartreflex_core: Calibration complete: Voltage Nominal=1127000 Calib=1012840 Dyn=1062840 OPP_margin=13000 total_margin=25320
[    0.376678] sr_classp5_calib_work: smartreflex_mpu: Calibration complete: Voltage Nominal=1203000 Calib=1025500 Dyn=1075500 OPP_margin=0 total_margin=0
[    0.376800] sr_classp5_calib_work: smartreflex_iva: Calibration complete: Voltage Nominal=950000 Calib=822940 Dyn=872940 OPP_margin=13000 total_margin=25320
[    0.500152] highmem bounce pool size: 64 pages
[    0.501403] fuse init (API version 7.18)
[    0.501617] msgmni has been set to 1165
[    0.503570] io scheduler noop registered
[    0.503601] io scheduler deadline registered
[    0.503662] io scheduler cfq registered (default)
[    0.504974] OMAP DSS rev 4.0
[    0.528320] d2l 2-000f: D2L i2c initialized
[    0.528503] omapdss DSI error: can't get regulator for panel
[    0.529144] dsscomp: initializing.
[    0.529205] misc dsscomp: found 2 displays and 4 overlays, WB overlay 1
[    0.530120] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 105) is a OMAP UART1
[    0.530578] omap_uart.2: ttyO2 at MMIO 0x48020000 (irq = 106) is a OMAP UART2
[    1.764801] console [ttyO2] enabled
[    1.769134] omap_uart.3: ttyO3 at MMIO 0x4806e000 (irq = 102) is a OMAP UART3
[    1.777435] [drm] Initialized drm 1.1.0 20060810
[    1.782684] omap_ion_probe: adding heap secure_input of type 2 with ba300000@5a00000
[    1.791107] omap_ion_probe: adding heap tiler of type 4 with b4300000@6000000
[    1.798889] omap_ion_probe: adding heap nonsecure_tiler of type 4 with a0200000@2000000
[    1.807556] omap_ion_probe: adding heap system of type 0 with 0@0
[    1.814208] omap_ion_probe: adding heap tiler_reservation of type 5 with 0@0
[    1.830200] brd: module loaded
[    1.837860] loop: module loaded
[    1.841369] (stk) :sysfs entries created
[    1.845672] (stk) : debugfs entries created 
[    1.850189] (hci_tty): inside hci_tty_init
[    1.854980] (hci_tty): allocated 252, 0
[    1.859130] AK8975 compass driver: init
[    1.866760] NFC Driver for TI WiLink
[    1.870697] (nfcdrv) nfc_drv_probe: allocated major 250, minor 0
[    1.878112] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.886016] omap2_mcspi omap2_mcspi.1: master is unqueued, this is deprecated
[    1.894134] omap2_mcspi omap2_mcspi.2: master is unqueued, this is deprecated
[    1.902221] omap2_mcspi omap2_mcspi.3: master is unqueued, this is deprecated
[    1.910339] omap2_mcspi omap2_mcspi.4: master is unqueued, this is deprecated
[    1.918395] tun: Universal TUN/TAP device driver, 1.6
[    1.923889] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[    1.931304] usbcore: registered new interface driver asix
[    1.937225] usbcore: registered new interface driver cdc_ether
[    1.943664] usbcore: registered new interface driver smsc95xx
[    1.949951] usbcore: registered new interface driver net1080
[    1.956176] usbcore: registered new interface driver cdc_subset
[    1.962646] usbcore: registered new interface driver zaurus
[    1.968749] usbcore: registered new interface driver cdc_ncm
[    1.975311] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.982788] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[    1.989257] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[    1.998840] ehci-omap ehci-omap.0: irq 109, io mem 0x4a064c00
[    2.017120] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[    2.023529] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    2.030914] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    2.038757] usb usb1: Product: OMAP-EHCI Host Controller
[    2.044525] usb usb1: Manufacturer: Linux 3.4.34 ehci_hcd
[    2.050384] usb usb1: SerialNumber: ehci-omap.0
[    2.055938] hub 1-0:1.0: USB hub found
[    2.060058] hub 1-0:1.0: 3 ports detected
[    2.095489] usbcore: registered new interface driver cdc_wdm
[    2.101623] Initializing USB Mass Storage driver...
[    2.107025] usbcore: registered new interface driver usb-storage
[    2.113555] USB Mass Storage support registered.
[    2.118652] usbcore: registered new interface driver libusual
[    2.124969] usbcore: registered new interface driver usbtest
[    2.131103] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    2.338836] musb-hdrc musb-hdrc: USB OTG mode controller at f0316000 using DMA, IRQ 124
[    2.347991] mousedev: PS/2 mouse device common for all mice
[    2.355438] twl6030_pwrbutton_probe: Enter
[    2.360198] input: twl6030_pwrbutton as /devices/platform/omap_i2c.1/i2c-1/1-0049/twl6030_pwrbutton/input/input0
[    2.373168] twl_rtc twl_rtc: Power up reset detected.
[    2.379852] twl_rtc twl_rtc: Enabling TWL-RTC.
[    2.392059] usb 1-1: new high-speed USB device number 2 using ehci-omap
[    2.425872] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[    2.432586] i2c /dev entries driver
[    2.436889] usbcore: registered new interface driver uvcvideo
[    2.443115] USB Video Class driver (1.1.1)
[    2.447692] Driver for 1-wire Dallas network protocol.
[    2.468505] twl6030_bci twl6030_bci: Battery Voltage at Bootup is 3791 mV
[    2.481964] omap-bandgap omap-bandgap: failed to fetch platform data
[    2.490570] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    2.499328] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[    2.510620] cpuidle: using governor ladder
[    2.515533] cpuidle: using governor menu
[    2.528991] omap4430_sdp_display_probe:Enter
[    2.534332] omap4430_sdp_display_probe:Exit
[    2.539337] usbcore: registered new interface driver usbhid
[    2.545593] usbhid: USB HID core driver
[    2.549896] thermal_get_slope:Getting slope is not supported for domain cpu
[    2.557495] thermal_get_offset:Getting offset is not supported for domain cpu
[    2.565155] usb 1-1: New USB device found, idVendor=0424, idProduct=9500
[    2.572357] omap_governor_init: domain cpu slope -22 const -22
[    2.578643] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[    2.587371] thermal_get_slope:Getting slope is not supported for domain gpu
[    2.597106] thermal_get_offset:Getting offset is not supported for domain gpu
[    2.604980] smsc95xx v1.0.4
[    2.608001] omap_governor_init: domain gpu slope -22 const -22
[    2.614898] rproc remoteproc0: ipu_c0 is available
[    2.620086] rproc remoteproc0: Note: remoteproc is still under development and considered experimental.
[    2.630310] rproc remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    2.642425] OMAP HSI: HSI driver version 0.4.4
[    2.647827] usbcore: registered new interface driver snd-usb-audio
[    2.658264] oprofile: using arm/armv7-ca9
[    2.662628] GACT probability NOT on
[    2.666381] Mirror/redirect action on
[    2.670288] u32 classifier
[    2.673156]     Actions configured
[    2.676788] Netfilter messages via NETLINK v0.30.
[    2.681945] nf_conntrack version 0.5.0 (10520 buckets, 42080 max)
[    2.688781] ctnetlink v0.93: registering with nfnetlink.
[    2.694549] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[    2.702087] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[    2.708557] xt_time: kernel timezone is -0000
[    2.713653] ip_tables: (C) 2000-2006 Netfilter Core Team
[    2.719635] arp_tables: (C) 2002 David S. Miller
[    2.724700] TCP: cubic registered
[    2.728302] Initializing XFRM netlink socket
[    2.733062] NET: Registered protocol family 10
[    2.738677] Mobile IPv6
[    2.741363] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    2.747436] IPv6 over IPv4 tunneling driver
[    2.752868] NET: Registered protocol family 17
[    2.757720] NET: Registered protocol family 15
[    2.762603] Bridge firewalling registered
[    2.767089] Bluetooth: RFCOMM TTY layer initialized
[    2.772369] mmc0: new high speed MMC card at address 0001
[    2.778533] mmcblk0: mmc0:0001 HBG4e 29.1 GiB 
[    2.778533] Bluetooth: RFCOMM socket layer initialized
[    2.778533] Bluetooth: RFCOMM ver 1.11
[    2.778533] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    2.778564] Bluetooth: BNEP filters: protocol multicast
[    2.778564] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    2.778656] NET: Registered protocol family 35
[    2.815521] NET: Registered protocol family 37
[    2.819427] smsc95xx 1-1:1.0: eth0: register 'smsc95xx' at usb-ehci-omap.0-1, smsc95xx USB 2.0 Ethernet, 0a:c0:6b:90:a2:29
[    2.832092] NET: Registered protocol family 40
[    2.832122] mmcblk0boot0: mmc0:0001 HBG4e partition 1 4.00 MiB
[    2.832305] mmcblk0boot1: mmc0:0001 HBG4e partition 2 4.00 MiB
[    2.834289]  mmcblk0: unknown partition table
[    2.837554]  mmcblk0boot1: unknown partition table
[    2.840576]  mmcblk0boot0: unknown partition table
[    2.864654] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    2.872924] ThumbEE CPU extension supported.
[    2.877532] Registering SWP/SWPB emulation handler
[    2.884277] sr_classp5_calib_work: smartreflex_mpu: Calibration complete: Voltage Nominal=1380000 Calib=1228060 Dyn=1278060 OPP_margin=0 total_margin=0
[    2.904541] clock: disabling unused clocks to save power
[    2.931884] mmc1: host does not support reading read-only switch. assuming write-enable.
[    2.942993] mmc1: new high speed SD card at address 0002
[    2.948883] mmcblk1: mmc1:0002 00000 1.86 GiB 
[    2.955657]  mmcblk1: p1 p2
[    3.058532] cannot apply mgr(lcd) on inactive device
[    3.063995] cannot apply mgr(lcd) on inactive device
[    3.069427] omapfb omapfb: failed to apply dispc config
[    3.075225] cannot apply mgr(tv) on inactive device
[    3.080657] omapfb omapfb: failed to apply dispc config
[    3.087463] cannot aply mgr(lcd2)--invalid device
[    3.094635] omapfb omapfb: failed to apply dispc config
[    3.100799] mmc2: card claims to support voltages below the defined range. These will be ignored.
[    3.137145] mmc2: error -110 whilst initialising SDIO card
[    3.332733] tc358765 display0: couldn't access LVPHY0, going on with reset value
[    3.350524] tc358765 display0: couldn't access VPCTRL, going on with reset value
[    3.358642] tc358765 display0: couldn't access LVCFG, going on with reset value
[    3.370727] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[    3.379516] ALSA device list:
[    3.382720]   No soundcards found.
[    3.386596] Waiting 2sec before mounting root device...
[    5.407440] EXT2-fs (mmcblk1p2): warning: mounting ext3 filesystem as ext2
[    5.414978] EXT2-fs (mmcblk1p2): warning: mounting unchecked fs, running e2fsck is recommended
[    5.430541] VFS: Mounted root (ext2 filesystem) on device 179:26.
[    5.437316] Freeing init memory: 352K
[    5.443756] Failed to execute /init.  Attempting defaults...
INIT: version 2.86 booting
Error Cannot open /dev/tty0: No such device or address
Please wait: booting...
Starting udev
[    6.222320] udevd (111): /proc/111/oom_adj is deprecated, please use /proc/111/oom_score_adj instead.
[    7.159393] HDCP: failed to load keys
[    7.159393] 
[    7.346496] FAT-fs (mmcblk0): bogus number of reserved sectors
[    7.352691] FAT-fs (mmcblk0): Can't find a valid FAT filesystem
[    7.449066] EXT4-fs (mmcblk0): VFS: Can't find ext4 filesystem
[    7.519073] EXT4-fs (mmcblk0): VFS: Can't find ext4 filesystem
[    7.573760] EXT2-fs (mmcblk0): error: can't find an ext2 filesystem on dev mmcblk0.
[    7.605194] FAT-fs (mmcblk0): bogus number of reserved sectors
[    7.611541] FAT-fs (mmcblk0): Can't find a valid FAT filesystem
[    8.092468] FAT-fs (mmcblk0boot0): bogus number of reserved sectors
[    8.099304] FAT-fs (mmcblk0boot0): Can't find a valid FAT filesystem
[    8.106658] FAT-fs (mmcblk0boot1): bogus number of reserved sectors
[    8.113464] FAT-fs (mmcblk0boot1): Can't find a valid FAT filesystem
[    8.153900] EXT4-fs (mmcblk0boot0): VFS: Can't find ext4 filesystem
[    8.208160] EXT4-fs (mmcblk0boot1): VFS: Can't find ext4 filesystem
[    8.263214] EXT4-fs (mmcblk0boot0): VFS: Can't find ext4 filesystem
[    8.318023] EXT4-fs (mmcblk0boot1): VFS: Can't find ext4 filesystem
[    8.353149] sr_classp5_calib_work: smartreflex_mpu: Calibration complete: Voltage Nominal=1025000 Calib=822940 Dyn=872940 OPP_margin=10000 total_margin=12660
[    8.372528] EXT2-fs (mmcblk0boot0): error: can't find an ext2 filesystem on dev mmcblk0boot0.
[    8.427276] EXT2-fs (mmcblk0boot1): error: can't find an ext2 filesystem on dev mmcblk0boot1.
[    8.474121] FAT-fs (mmcblk0boot0): bogus number of reserved sectors
[    8.480926] FAT-fs (mmcblk0boot0): Can't find a valid FAT filesystem
[    8.521270] FAT-fs (mmcblk0boot1): bogus number of reserved sectors
[    8.528076] FAT-fs (mmcblk0boot1): Can't find a valid FAT filesystem
[    8.812957] alignment: ignoring faults is unsafe on this CPU.  Defaulting to fixup mode.
Remounting root file system...
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
ALSA: Restoring mixer settings...
Configuring network interfaces... ifup: ignoring unknown interface usb0
done.
Setting up IP spoofing protection: rp_filter.
/usr/sbin/alsactl: load_state:1625: No soundcards found...
Fri Dec 23 00:37:00 UTC 2011
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project http://arago-project.org dm37x-evm ttyO2

Arago 2011.06 dm37x-evm ttyO2

dm37x-evm login: �ootڈ�����������
 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project http://arago-project.org dm37x-evm ttyO2

Arago 2011.06 dm37x-evm ttyO2

dm37x-evm login: �oot�
                      P���wor�:�o�i�̠ti�e��o�t��fter�60��eco��


Í