U-Boot SPL 2013.04 (Feb 07 2014 - 10:54:33)
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.04 (Feb 07 2014 - 10:54:33)
AM35XX-GP ES2.0, CPU-OPP2, L3-165MHz, Max CPU Clock 600 Mhz
CraneBoard + LPDDR/NAND
I2C: ready
DRAM: 256 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0
In: serial
Out: serial
Err: serial
Die ID #4294000100000000015da3960401c020
Hit any key to stop autoboot: 0
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading uImage
2991208 bytes read in 268 ms (10.6 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.8.13
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2991144 Bytes = 2.9 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
I am trying to port linux-3.8.13 in craneboard.
but After this massage kernel hangs?
I can able to run linux-2.6 but I want to run 3.8 for crane board?