I have the DK-TM4C123G Dev boards - the ones with the 96x64 OLED display and I'm in process of getting everything in my IDE up to date. I've just gone up to CCS5.5.0.00077 and, because I want only to work with Tiva processors (at present), I installed TI-RTOS 1.10.00.23 which was suggested in the prep for the TI-RTOS training stuff done by Eric W.
However, the UG file in my docs folder under C:\ti\tirtos_1_10_00_23\docs is spruhd4c.pdf which - in section 1.1 - does not list the DK-TM4C123G dev board as one for which there are examples. Reading documents onine, I found http://www.ti.com/lit/ug/spruhd4e/spruhd4e.pdf which is a more up to date version of the UG document.
Do I need to update my version of TI-RTOS to something higher than 1.10.00.23 to see the DK-TM4C123G example(s)?
If yes, what's the link?
Thanks :D