Hi There,
I have a 1920x1080 active size sensor output and from that i convert it into the YCbCr 4:4:4 format.
Now i want to convert YCbCr 4:4:4 output into 1080p BT-656 (YCbCr 4:2:2) interface specific,so should i have to transfer it in the two field (odd-even field) form like NTSC and PAL or i can output a frame as a whole like other BT interface standard?
Please reply.
Regards,
Hitesh