We are using the OMAP2420 SDP. Please find the details below.
We used CSST but found doesn't have siupport to flash ES1.0 boards. Hence tried using OST. We are able to flash the LED blink raw files.
We tried flashing the UBOOT.BIN, But unable. Does any one knows the complete tools set and uboot, Linux image and file system and the procedures documented.
Thanks ... Suresh
= O S T BOOT Console [OMAP242X SDP] - 1.10 Apr 21 2008 19:21:32
Silicon Revision Number - ES 1.0
Displaying Main Board EEPROM contents
EEPROM Data Format Version - 0100
Platform Information Version - H400
Board Number - 700-0561-000
Board Revision - 0C02
Manufacture Date - 112004
Board Serial Number - 00006328
Displaying Daughter Board EEPROM contents
EEPROM Data Format Version - 0100
Platform Information Version - H400
Board Number - 700-0680-000
Board Revision - 0A04
Manufacture Date - 022005
Board Serial Number - 00006800
Combo Device Memory Device Speed Grade - 000
Discrete SDR Device Speed Grade - 105
----------------------------------------------------------------------
OSTBOOT>