This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCDK6848 and webcamera

Hi everyone.

I’m working with the LCDK6748. I’m wondering if a web camera can be attached to the LCDK6748 in the USB Host port using a windows driver. Is this possible?

Thank you very much.

  • Hi llich Guerrerro,

    llich Guerrerro Says said:
    I’m working with the LCDK6748. I’m wondering if a web camera can be attached to the LCDK6748 in the USB Host port using a windows driver. Is this possible?

    yes, it is possible to connect the USB webcamera into the C6748 LCDK as it has a USB Host port. And you have to have your USB device class driver for webcamera ( UVC) keep running to make it work.

    Regards,

    Shankari

     

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------

  • Shankari

    Thank you very much. Let me try to find out the way to perform it.

    I'll be in touch