This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5509A connection error from CCS 3.1

Dear,

Now I am testing the ECG board using TMS320C5509A by designed myself, and I connect  to this DSP from CCS 3.1 by pressing Alr+C, I got the following message:

///////////////////
It appears that the target is being held in reset.  This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings.  If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration

If this is a multi-core system, the master CPU may not be
releasing the DSP/MCU from reset.  Please check your
configuration in CC_setup and/or your GEL file to ensure that
nothing is blocking the DSP/MCU from being released from reset

///////////////////
I use Spectrum Digital XDS510USB PLUS debugger to test JTAG connection, it is OK.
I also monitor the clockout from DSP after reseting, there is oscillation on this CLOCKOUT pin at frequency 12 MHz (the same frequency at pin X1/X2CLKIN).


If anyone has a solution for this, please advise me.

Thanks,

Phung Van Ha