Other Parts Discussed in Thread: OMAP-L138
We're investigating booting the LINUX kernel over USB. Can someone point me to resources on this topic? Is this available for both the OTG USB port and the host port?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What processor are you using?
for OMAP-L1, there is some information at:
http://tiexpressdsp.com/index.php/Alternate_Boot_Methods_for_OMAP-L137/DA830#From_USB_storage
Hi Mariana,
Did you try to boot Linux from USB (OTG) in OMAP-L138 Experimenter Kit board (Logicpd)?
If the answer is yes, Which version of Linux & PSP did you use?
I'm asking you because when Linux boot from USB then the stick is not recognized (PSP: ti-dvsdk_omapl138-evm_4_00_00_22 and 4_01_00_09)
Any help will be appreciated.
Regards,
Marcelo