I want to use both SPI0_CS0 and and SPI1_CS1 using the McSPI module. Master mode only. I don't see any bit in registers to choose whether SPI_CS0 or SPI_CS1 is asserted when SPIEN is asserted. Where is it? I searched the whole technical manual and can't find it. Can someone point me to the spot?