Other Parts Discussed in Thread: TLV320AIC3106
All:
My aim is to use StarterWare v1.20.04.01 for the C6748. As a test, I've been trying to run an example audio pass through program that is provided with the TMDXLCDK6748 but have had no success getting audio through to my powered speakers.
Currently using line-in for the test tone input (from PC headset port) and line-out to get the output audio to speakers. Here are the approaches tried this far:
1) Created CCv5.3 project using source files found in C:\ti\C6748_StarterWare_1_20_04_01\examples\lcdkC6748\mcasp. When I built this example program (no modifications) it built with no errors but I could not get the input tone out of the LCDK to my speakers.
2) I created an empty CCS v5.3 project and copied C:\ti\C6748_StarterWare_1_20_04_01\binary\c674x\cgt_ccs\c6748\lcdkC6748\mcasp\Release\mcaspPlayBk.out to my empty project Release folder. I then used CCS v5.3 to load this prebuilt version of the example program to the LCDK and run it. Again, no success.
Any thoughts on what could be going wrong here?
Sincerely,
John Demery