Other Parts Discussed in Thread: OMAP-L138
Hi,
I've encountered a problem trying to get started with the L138 eXperimenter board. I've connected to the board from a Windows PC running Tera Term but when I power the board up I get
U-Boot 2009.01 (Jul 30 2009 - 11:58:01)
DRAM: 64MB
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 300000000 Hz
Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
U-Boot >
i.e. Linux has not been booted.
If I enter 'boot' at the command prompt, nothing happens.
Is the bad CRC message relevant?
I have two boards and both give exactly the same result (including CRC message).
Donald