This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Faced a QMSS problem in 6616 when send packets using multiple buffer descriptors.

Hi all:

          I faced a QMSS problem in 6616 when send packets using multiple buffer descriptors.
When I send a packet using 1 packet descriptor linked 2 buffer descriptor, which shows bellow

|-----------------------------|            |----------------------------|                 |-----------------------------|

|  Packet descriptor     |   ----->| Buffer descriptor1    |  ---------> |  Buffer descriptor2    |

|-----------------------------|            |----------------------------|                 |-----------------------------|

     The packets send out are error with Buffer descriptor1 Linked data remained the same for several times.

For example: we supposed the data in Buffer descriptor1 in first packet is 2, and we added the data by 1 for each packet, the folloing sending data will be 2,2,2,2,2,2,9,9,9,9,13,13,13, while the right data sequence should be 3,4,5,6,7,8,9,10,11,12,13,14,15...

     When I store the three descriptors's data to one descriptor and send out the data, the sending data sequence is right 

|-----------------------------|

|  Packet descriptor     |   

|-----------------------------|  

  So I dont know why this happens?Is anybody meet such problem?I will preciate your help very much.

  • Hi Figo,

    TCI66xx devices such as TCI6616 are supported directly through Local Field Applications Engineers (FAEs.)  These devices are not supported on the E2E forum.  Please contact your local FAE for support of these devices.  If you are not sure who your local FAE is, then please contact your local technical sales representative and they will be able to put you in contact with your local FAE.

    Otherwise, Please provide below information.

    What is the device part number? Are you working on EVM or Custom Board? If EVM, what is the part number?