This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L2 cache of DM6437

I didnt quiet understand the size of the L2 cache is DM6437. In the manual it says that 128 KB of L2 memory can be configured as SRAM or cache or combination of both. Then it also says there is 2 MB of SRAM that contributes to the memory map. Cant we assign this 2 MB of SRAM as L2 cache ?