This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 field decode & encode



Hi

      Can DM368 support field encode and decode in H.264 ? Fifstly,encode odd field .Then encode even field.

      Dvsdk_dm368_4_02_00_06 is be used.

  • Hi,

    Yes it supports Field encode and decode in H264. Currently it supports only top(even) filed first. 

    If you need bottom(odd) filed first, you can try by giving bottom field as top field to the encoder. For more info please refer the below link on Filed(Interlaced) encoder.

    http://processors.wiki.ti.com/index.php/DM36x_Interlace_Encoding_FAQs