This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EzDSP ADC



Hi,

I'm trying to get the ADC going on EzDSP. I set up everything as per the application note and once the busy flag is cleared I read the data. For some reason the data is always 0xff even i ground the input pin (GPAIN0).

Does anyone have some sample code that could be help.

Any help very much appreciated.


Regards

 

  • Hi Avvi,

    You should check out the example projects included in the C5505 Chip Support Library.

    For C5505 eZdsp, you need to download C55XCSL-LOWPOWER from http://focus.ti.com/docs/toolsw/folders/print/sprc133.html

    Once installed, the following three ADC examples will be located under <install path>\VC5505_CSL\CCS_v4.0_Examples\sar\ :

    CSL_SAR_DmaExample
    CSL_SAR_IntcExample
    CSL_SAR_PollExample


    These projects should get you started with the ADC. Please be sure to read the Release Notes that get installed with the CSL for CCS4.0 usage instructions.

    Let us know how it goes.

    Thanks,
    Mark

     

     

  • Thanks Mark,

    Just managed to put in some more time into last few days - it works like a charm! Excellent stuff!

    Appreciate the help.

    Regards