This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm642



Hi frnds,

I'm working on EVMDM642 board with CCSv5 using blackhawk XDS510USB2.0Plus emulator, the target configuration was done, after launching my configured target file i tried to connect while connecting it shows the following error for first time

Error connecting to the target:
(Error -115 @ 0x0)
A bad parameter value passed to a function was detected.
The controller or software would later enter an invalid state.
(Emulation package 5.0.872.0)

then i reset the board using reset button and tried to connect then it shows the  error message as

 

Error connecting to the target:
(Error -121 @ 0x0)
A bad controller handle has been given to a function,
either before attempting to open the controller, or after
having opened the controller and ignored its error status.
Valid controller handles are generated when attempts
to open the controller return a clean error status.
(Emulation package 5.0.872.0)

now i want to know what is the problem happening with the board. the emulator is working fine with the other dsp boards,

if anybody know the solution kindly help me thanks in advance