This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x GPMC configuration in linux SDK

I am using am335x with linux. the SDK is ti-sdk-am335x-evm-05.05.00. I use the am335x to communicte with one nand and the FPGA. when I use the gpmc port to communicate with FPGA. I read the register of GPMC_CONFIG7_0-GPMC_CONIFG7_6. I find the base address is 0x8000000,0x1000000,0x2000000,0x3000000,0x4000000,0x5000000,0x6000000 and the maskaddress is 16M.

the question is I do not configure the register of GPMC_CONFIG7_i.

if I want to configure the register, how to configure them is the SDK of  ti-sdk-am335x-evm-05.05.00.

thank you!