This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bug report: CSLR in the C6657 PDK v1.1.2.6

Hello,

I'd like to report a bug with the C6657 PDK.

If we look at the PDF describing the PCIe core (SPRUGS6B), we can see the following: 

Section 3.2.2 Vendor and Device Identification Register (VENDOR_DEVICE_ID)
Bits[31:16] DEVICE_ID, Default Value: Unknown
Bits[15:0] VENDOR_ID, Default Value: 0x104C

Now, let's look at some files within the 6657 PDK.

/opt/ti/pdk_C6657_1_1_2_6/packages/ti/csl/cslr_pcie_cfg_space_endpoint.h

#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_MASK     (0xFFFF0000u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_SHIFT    (0x00000010u) 
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_RESETVAL (0x00008888u)

#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_MASK     (0x0000FFFFu)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_SHIFT    (0x00000000u) 
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_RESETVAL (0x0000104Cu)

/opt/ti/pdk_C6657_1_1_2_6/packages/ti/csl/cslr_pcie_cfg_space_endpoint.h

#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_MASK     (0xFFFF0000u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_SHIFT    (0x00000010u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_RESETVAL (0x00008888u)

#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_MASK     (0x0000FFFFu)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_SHIFT    (0x00000000u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_RESETVAL (0x0000104Cu)

These definitions do not agree with the documentation. By testing with real hardware, it is clear that the documentation is correct, and the CSL is incorrect. In both of these files, the correct definition would be:

#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_MASK     (0x0000FFFFu)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_SHIFT    (0x00000000u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_VENDOR_ID_RESETVAL (0x0000104Cu)

#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_MASK     (0xFFFF0000u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_SHIFT    (0x00000010u)
#define CSL_PCIE_CFG_SPACE_ENDPOINT_VENDOR_DEVICE_ID_DEVICE_ID_RESETVAL (0x00008888u)

Enjoy,
Bill Lynch