Other Parts Discussed in Thread: OMAP-L137
DO OMAPL137 must use NDK2.0 ? IF OMAPL137 can use NDK2.21.01.38 and NSP 1.10.01.06 ? if can use NDK2.21.01.38 and NSP 1.10.01.06,how to modify it to adapt the OMAPL137.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L137
DO OMAPL137 must use NDK2.0 ? IF OMAPL137 can use NDK2.21.01.38 and NSP 1.10.01.06 ? if can use NDK2.21.01.38 and NSP 1.10.01.06,how to modify it to adapt the OMAPL137.
Hi,
Yes, this release (NDK2_0_0) includes some sample platform specific code and example projects for C6747 / OMAP-L137 devices. NDK 2.00 release include TCP/IP stack source and binarys and associated NSPs (drivers).
Please check the device web page for NSP (Ethernet driver package) updates or download the driver from the NDK 2.00 full package. Find the NDK and NSP download link avilable at this wiki: http://processors.wiki.ti.com/index.php/Before_asking_for_NDK_support
You can refer more details at the release notes of NDK and NSP.
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ndk/2_21_01_38/exports/ndk_2_21_01_38/ndk_2_21_01_38_ReleaseNotes.html
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ndk/nsp_1_10_01_06/exports/nsp_1_10_01_06/nsp_1_10_01_06_release_notes.html
I know this is an old thread and sorry for resuscitating it but the ndk 2.21 nor the nsp 1.10 have support for the OMAP-L137 but the 138. I'm interested in drivers supports for the 137 for the ndk. Are those available? or would I have to resort to porting the code over. I need the ndk support for the arm9 side which seems to be available in the 138 example but I would prefer to double check if there is something specifically available, even if it is not supported, for the 137.