Hi everyone,
Currently running the Appro 2A software library on the dm365 platform, using MT9P031 senssors. I was just wondering what the default frame rate the Appro 2A library is expecting and how do we configure this setting. I was looking at the IPNC code that is provided with the Appro library, and notice that it sets the frame rate in one of its global structure to zero. Unfortunately it has no documentation on what this value means, that I can see. Any help would be most appreciated. Thanks.