Other Parts Discussed in Thread: OMAPL138
Hi,
I have compiled the starterware Ethernet echo and Ethernet LWIP code .
When I use the command file provided by starterware following is the result.
The problem is when I debug the the program, the Debug window shows that there are no symbols defined.
When I use the command file generated by OMAPL138 following the result:
Although in the debug window displays the symbols _c_init_00 and main , when i try running and pause the program it shows there are no symbols to defined .
I have attached linker commands files provided by staterware and autogenerated