This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code porting to new Sitara ICAM3359 V2.1B

Other Parts Discussed in Thread: AM3359, SYSBIOS

Hi,

We have developed one application on ICE3359 board version 1.0A. Then somehow the board stopped working. It is not getting detected over USB at all.

So, we purchased new ICE board. This time we got the AM3359 ICE board revision 2.1A

No when I try to connect the debugger for this new board it is giving following errors

CortxA8: Breakpoint Manager: Retrying with a AET breakpoint

CortxA8: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x8001d704: (Error -1066 @ 0x333C) Unable to set requested breakpoint in memory. Verify that the breakpoint address is in writable memory. (Emulation package 5.1.73.0)

CortxA8: Breakpoint Manager: Retrying with a AET breakpoint

CortxA8: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x8000c9dc: (Error -1066 @ 0x333C) Unable to set requested breakpoint in memory. Verify that the breakpoint address is in writable memory. (Emulation package 5.1.73.0)

Is there any change in Rev 2.1 ICE board? Can anyone please guide us on this? Same code was running and working fine on V1.0A ICE board.

 

Thanks & Regards

-Balwant