Hi, all
I'm using dm365 Ti's gstreamer plugins TIVidenc1 to do h.264 encoding. I've two stream pipeline, both are h.264 encoder. The first h.264 encoder for 720P works fine, but the 2nd encoder for CIF resolution has a serious flickering problem. I analysis the encoded stream frame by frame with a h.264 stream tool. I found that the flicking occurs at each I frame after all P frame in a period. The YUV file and encoded file are attached here. I 've set the h.264 encoder with high quality and high speed, but the result is the same.
Pls help me, thanks!