Other Parts Discussed in Thread: OMAP-L137
Hi,
I am fairly new to using Linux and I am trying to load Linux on an OMAP-L137 EVM board. I have downloaded REL_LSP_02_20_00_07 and worked through the instructions in 'LSP_02.20_OMAP-L137_User_Guide.pdf' which was in the download. I have flashed uboot and that works fine and I get all the messages as described on the console.
The aim was then to boot the Linux kernel from SPI flash (section 3.6.2). The section talks about downloading the pre-built RAM disk image which is provided in the MontaVista tools installation. I have installed 'mvl_5_0_0_demo_lsp_setuplinux_02_20_00_07.bin' which was in the download. However, there is no ramdisk.gz in there that I can find. Also the tree referred to in the instructions '/pro/devkit/arm/v5t_le/target' does not exist. All that I can see is 'pro/devkit/lsp/ti-davinci'.
Have I downloaded the wrong thing and if so where do I find the pre-built ramdisk.gz that I need for the OMAP-L137?
Thanks.