Hello:
Now i am Confused by 5 port Ethernet switch in 66ak2h06, In my project i need to output 4 x GigE Simultaneously by SGMII interface, and they will work all the time, can i do so?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Changshui Li,
Yes. You can use 4 SGMII Interface ports available in 66AK2H06. Please refer the 66AK2H06 datasheet and product folder for more information.
Datasheet: http://www.ti.com/lit/ds/symlink/66ak2h06.pdf
Product Folder: http://www.ti.com/product/66ak2h06
Thanks.
NETCP is connected to DSP cores via Teranet, see "7.3 TeraNet Switch Fabric Connections Matrix - Configuration Space" of 66AK2H14/12/06 Multicore DSP+ARM KeyStone II System-on-Chip (SoC) (Rev. E) datasheet. The bandwidth is far beyond 1Gb/s. You can use 4 SGMII port with 1.0Gb/s each.
Regards, Eric
Whilst NETCP is connected to the DSPs and ARMs via Teranet the only connection between NETCP and the SGMII ports appears to be via the host port of the GbE switch which is limited to 1Gb/s.
See:
KeyStone Architecture
Gigabit Ethernet (GbE) Switch Subsystem
Figure 1-2 KeyStone II Ethernet Switch Subsystem Block Diagram
That would suggest that it is not possible to transmit/receive data at more than 1Gb/s via the 4 SGMII ports as the OP and I want to do.
Do I understand this correctly or is there some way to transmit/receive data directly from the SGMII bypassing the GbE switch?