This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about the scale mode of DEI link

Hi TI experts,

    Env: 8168evm, rdk 4.1.

I have one question about the scale mode of DEI link:

assume the input resolution of dei link is 1024*768, and the user want the output resolution is 1920*1080, and the user want the content of output frame like below:

1)  frame 1024*768 upscaled to 1440*1080;

2)  the 1440*1080 in the middle of output frame content.

Can this function be implemented? How to do it?

Thanks