This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDHC Driver - OMAP 3503



Hello All,

I am working on the device that was based on OMAP3503DCUS Processor running on Win CE 6.0 R2. The device was designed to support two micro SD slots. Internal and External Slots.

                 There was a requirement in order to make the device supporting the Wi-Fi SDHC Cards by replacing the external micro SD card. We made an add-on card for interfacing micro SD with SD form factor. Many test cases related to detection, Read/Write etc. have been formed to check all sort of Wi-Fi as well as normal SDHC cards. Now the issue is that the device fails in reading most of the cards thus would not be mounted. Please refer to the following test results.

 

Type of Card

Result

Transcend Class 4 SDHC Cards (4GB,8GB)

Success

Transcend Class 10 SDHC Cards (8GB)

Success

SanDisk 2GB SDHC Card

Fail

Toshiba Flash Air Class 6 Wi-Fi SDHC Card (8GB)

Fail

Toshiba Flash Air Class 10 Wi-Fi SDHC Card (8GB)

Fail

Transcend Class 10 Wi-Fi SDHC Card (16GB)

Fail

 The same add-on card when connected to the Internal slot, all the cards were detected without any issue.

 The main difference between Internal and External slots is that the Internal slot was connected to the in-built Transceiver of the processor whereas the external slot was connected to the external transceiver (TI’s SN74AVCA406DGGR). On debugging the SDHC driver code, it was found that there exists Data CRC error. The status of MMCHS_STAT register was not set properly that BRR (Buffer Read Ready) bit was not set. Even the block length argument was improper in the command send to Host Controller where this was not the case with detected cards. Even we had tried with different clock frequencies but in vain.

                Please respond if someone faced the same issue and had a solution.

Thanks in Advance

  • Hello,

    There is a separate forum dedicated to OMAP3 devices: OMAP35x Processors Forum (http://e2e.ti.com/support/dsp/omap_applications_processors/f/447.aspx?pi74949).

    Could you please post this question there? It is out of the scope of OMAP Application processors (OMAP4 & OMAP5);

    Thanks,

    Yordan