This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pixel Aspect Ratio DM8168

We use DVRRDK 03/04 and own Udworks based hardware design.

We want to use 4:3 and also 16:9 displays at SD video output.

So as I understand SAR / PAR / DAR we have the following relations:

SAR (Storage aspect ratio) = 720:576 = 5:4

DAR (Display Aspect Ratio) is 4:3 or 16:9

PAR (Pixel Aspect Ratio) = DAR/SAR -->

(4:3)/(5:4) = 16:15 = 1,067

or (16:9)/(5:4) = 64:45 = 1,42

This means we have to set PAR to the related values if we want to change between 4:3 and 16:9.

Is it possible to set Pixel Aspect Ratio in DM8168 ?