Which path variable do you have to edit if you want to run the QualiTI application? I keep on getting the "xs command not in the path, giving up ..." error message, but no matter where I specify the path it does not seem to work even though the files exist where they should be.
Where in the startqti.sh file, but also elsewhere do you point to the additional path?