This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DVRRDK linux kernel patches



Hi,

TI has declared the EZSDK to be NRND over at http://www.ti.com/tool/linuxezsdk-davinci, and recommended the use of the RDK.  So we have started looking into the DVRRDK 04.01.00.02.

The DVRRDK documentation claims that the kernel comes from Arago, the 2010.06_TI81XXPSP_04.04.00.02.pacth1 release.  But when I compare the kernel to what's in Arago I find that it has additional changes.  Some of these changes look like Arago changes, and are probably described by the patches contained with the RDK at DVRRDK_04.01.00.02/ti_tools/linux_lsp/kernel/linux-dvr-rdk/temp/.  But there appear to be other RDK-specific changes as well, like customization for the MACH_UD8168_DVR.  Are the individual patches for these commits available?  Or, is there some git repo for the DVRRDK version of u-boot and kernel where I can get the patches myself?

Also - how can we know when there is a new version of DVRRDK available?  Is there a place where this is announced?  Or do we have have to continually pester our FAE for status updates?

Thanks,

Dan -