This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: CAD Symbols and Footprints for DRV2667 and AFE440

Other Parts Discussed in Thread: AM3357, AFE4400

Janet,

Thank you for the updated file and I look forward to receiving the AFE4400 file. I have recently started having issues with the AM3357. I am trying to connect it to external NAND Flash through the MMC. The datasheet indicates that it has up to 3 MMC ports with an 8-bit mode. However, the pin map only shows one 4-bit port as does the CAD symbol leaving the last 4 bits of the Flash memory floating. Am I missing something? Is there a GPIO that I am not seeing that has an MMC mode and allows the AM3357 to support an 8-bit port?

Thanks,

Imran