Hi folks,
We are trying to enable the ROI feature on the H264 encoder. Our platform is as follows:
1. DM8127 processor
2. H.264 Encoder version 02.00.02.02.
Firstly, does ROI function correctly on this version of the encoder?
When we try to enable ROI on the encoder (by setting the enableROI flag in the dynamic params) we are finding that, when we read the encoder status back the enableROI flag is always set to zero. There is no error being reported from any of the function calls.
My understanding is that there are certain combinations of H.264 parameters that cause ROI to be automatically disabled. Is there are definitive list available?
I can supply a list of our current settings if need be.
Any help would be appreciated with this problem,
Thanks in advance,
Regards,
Terry