Hello,
We have a customize board based on DM8148 and we are using RDK 4.0 on it.
We are giving
1] 8ch capture + encode + dump (mp4 + JPEG)&
2] 8ch capture + display support.
Now we are migrating on RDK 4.1 because of B Frame support.
But, after migrating, what we have observed is that in each gop initial two frames are very large compare to RDK 4.0.
And might be because of this, file size also increase.
Is there any setting for this? Because we are not getting these large frames in starting of gop in RDK 4.0.