This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dei link set

hi all .i see the dei link can output 420 yuv ,but now when i link the dei to enc link directly ,it has below error:

so how can i fix the problem 

[m3vpss ] 13508: CAPTURE: Start Done !!!
[m3video] 13509: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3video] 13511: IPC_IN_M3 : Create Done !!!
[m3video] 13511: ENCODE: Create in progress ... !!!
[m3video] 13572: ENCODE: Creating CH0 of 1920 x 1080, pitch = (3840, 3840) [PROGRESSIVE] [NON-TILED ], bitrate = 2000 Kbps ...
[m3video] 13572: Assertion @ Line: 758 in links_m3video/iva_enc/encLink_common.c: pChAlgCreatePrm->inputChromaFormat == XDM_YUV_420SP : failed !!!

 

 

another question is that i see the NSF can change the resolution dynamiclly in the DVR_RDK_McFW_Link_API_Training.pdf,so how to do it ,i can not see the resolution in the NSF structure