This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Edge Enhancer LUT memory location



Hi,

Is the memory location of this LUT hardcoded in hardware or is there a register setting somewhere that we can change it? Thanks.

 

  • It appears to be fixed, at least I was not able to uncover any register that changes the LUT address.

    In general I am not sure why you would need to change the memory location of the LUT outside of the specialized edge enhancement peripheral's memory?

  • Thanks for the reply. I had an idea that it would be fixed, but just wanted to verification. The reason why I would need to change this value is because I'm working on an application that would mux 2 sensor streams through the dm365, but the large number of values to set in the LUT is preventing me from setting this on a frame by frame basis.