Hi all:
I download TI81XX-LINUX-PSP-04.04.00.02.tgz to run the TI81XX PSP PCI Express Endpoint Boot Driver.
followed TI81XX_PSP_PCI_Express_Endpoint_Boot_Driver_User_Guide.pdf,
i boot my ep mode.
But as a newer to pcie, i still have some questions :
1. How to use TI81XX-LINUX-PSP-04.04.00.02.tgz patches, so many pathces,
should i have to patch one by one to the kernel src code ?
2. Followed TI81XX_PSP_PCI_Express_Endpoint_Boot_Driver_User_Guide,
I boot my dm8168 ep from dm8168 rc successfully,
the qustions is how to use the driver at the userspace, there is no ep application interface then ?
3.How to enable EDMA transfer and MSI in this driver RC?
4.What about the EP side should i have to write a new driver for ep side?
5.when EP is boot from nand there is no pcie init is done in the u-boot, should i have to write this by myself?
Can someone answer me these qustions ?
best regards
xavier