Hello.
I have a question about length DQGATEH net. Length DQGATEH=Length CK+average Length DQS2 and DQS3
(CK+(DQS2+DQS2_N+DQS3+DQS3_N/4)) is written in the datasheet (SPRS403H december 2007 - revised june 2012). In my project I have only 1 DDR2 memory, so DQS2, DQS3 should be pull up/down through 1K resistor (page 212 datasheet). And in this page in scheme connection between DDR_DQGATE2 and DDR_DQGATE3 is drawn (for example for dm648 DDR_DQGATE2 - NC and DDR_DQGATE3 pull down through 1K resistor).
If it's really need connect DDR_DQGATE2 and DDR_DQGATE3 what is the length of this connection should be (should I add DQS2, DQS3 length? )?