This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 USB 1.1

Other Parts Discussed in Thread: OMAP-L138

Does the USB 1.1 port on the L138 require 24.9 series resistors and 15K pulldowns?  The Logic PD schematic has them, but there is no mention of them in any datasheet for the L138.  Also, most USB 1.1 implementation have 47pF to ground at the connector, but these are not present in the Logic PD schematic nor are the mentioned in the schematic.  Are the caps required?