This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 USB 2.0

Questions on USB 2.0 on the L138 (Table 3 of SPRUFM9C):

1.  Can USB0_ID pulldown for host mode be less than 10K:  6.49K?  This is just for parts consolidation.

2.  Is the USB0_VDDA12 cap value 0.1uF or 0.22uF (Logic PD Schematic).  Same question for SATA_REG pin.

3.  USB0_VBUS:  please explain the following:

For host mode of operation, pull-up the USB power signal on the USB connector to 5V also.  Shouldn't it just be a connection to the 5V USB supply?

Also, for host-only mode, should USB0_VBUS be pulled (through a 1K resistor) directly to the always-on 5V supply, or the USB 5V supply that can be turned off?