This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SGX build on DM3730 based beagleboard-xm

Hi,

We are trying to get latest SGX 4.10.00.01 on beagleboard-xm. Linux version on beagle board-xm: 3.4.7

Here are the steps:

1. Build and install latest Graphics SDK using command:

make BUILD=release OMAPES=5.x SUPPORT_XORG=1 PM_RUNTIME=1 all

make BUILD=release OMAPES=5.x SUPPORT_XORG=1 PM_RUNTIME=1 install

2. On target, run /etc/init.d/omap-demo.

Here is the output:

X.Org X Server 1.12.0
Release Date: 2012-03-04
X Protocol Version 11, Revision 0
Build Operating System: Linux 2.6.35-30-generic-pae i686
Current Operating System: Linux Freezer01 3.4.7-x1 #50 SMP Thu Feb 27 12:08:47 IST 2014 armv7l
Kernel command line: console=ttyO2,115200n8 splash quiet text vram=12MB omapfb.mode=dvi:640x480MR-16@60 omapfb.vram=0:4M,1:3M,2:3M omapdss.def_disp=dvi root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait fixrtc mpurate=auto buddy=none buddy2=none
Build Date: 05 July 2013 03:04:09PM

Current version of pixman: 0.24.4
Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/usr/local/XSGX/var/log/Xorg.0.log", Time: Thu Feb 27 16:18:54 2014
(++) Using config file: "/usr/local/XSGX/etc/xorg.conf"
(==) Using config directory: "/etc/X11/xorg.conf.d"
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
(==) ServerLayout "ServerLayout0"
(**) |-->Screen "Screen" (0)
(**) | |-->Monitor "<default monitor>"
(**) | |-->Device "Video Device"
(==) No monitor specified for screen "Screen".
Using a default monitor configuration.
(==) Not automatically adding devices
(==) Not automatically enabling devices
(WW) The directory "/usr/local/XSGX/share/fonts/X11/TTF/" does not exist.
Entry deleted from font path.
(WW) The directory "/usr/local/XSGX/share/fonts/X11/OTF/" does not exist.
Entry deleted from font path.
(==) FontPath set to:
/usr/local/XSGX/share/fonts/X11/misc/,
/usr/local/XSGX/share/fonts/X11/Type1/,
/usr/local/XSGX/share/fonts/X11/100dpi/,
/usr/local/XSGX/share/fonts/X11/75dpi/
(==) ModulePath set to "/usr/local/XSGX/lib/xorg/modules"
(==) |-->Input Device "Keyboard"
(==) |-->Input Device "<default keyboard>"
(==) The core pointer device wasn't specified explicitly in the layout.
Using the first mouse device.
(==) The core keyboard device wasn't specified explicitly in the layout.
Using the default keyboard configuration.
(II) Loading /usr/local/XSGX/lib/xorg/modules/extensions/libextmod.so
(II) Module extmod: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.0.0
(II) Loading /usr/local/XSGX/lib/xorg/modules/extensions/libdbe.so
(II) Module dbe: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.0.0
(II) Loading /usr/local/XSGX/lib/xorg/modules/extensions/libglx.so
(II) Module glx: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.0.0
(==) AIGLX enabled
(II) Loading /usr/local/XSGX/lib/xorg/modules/extensions/librecord.so
(II) Module record: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.13.0
(II) Loading /usr/local/XSGX/lib/xorg/modules/extensions/libdri.so
(II) Module dri: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.0.0
(II) Loading /usr/local/XSGX/lib/xorg/modules/extensions/libdri2.so
(II) Module dri2: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.2.0
(II) Loading /usr/local/XSGX/lib/xorg/modules/drivers/pvr_drv.so
(II) Module PVR: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 110.235.9475
(II) Loading /usr/local/XSGX/lib/xorg/modules/input/evdev_drv.so
(II) Module evdev: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 2.6.0
(II) Loading /usr/local/XSGX/lib/xorg/modules/input/kbd_drv.so
(II) Module kbd: vendor="X.Org Foundation"
compiled for 1.12.0, module version = 1.6.1
(II) pvr: Driver for PowerVR chipsets: PowerVR SGX
(--) using VT number 7

(WW) xf86OpenConsole: setpgid failed: Operation not permitted
(WW) Falling back to old probe method for pvr
FATAL: Module pvrsrvkm not found.
(EE) Couldn't get PVR Services status
(EE) No devices detected.

Fatal server error:
no screens found

Please consult the The X.Org Foundation support
at http://wiki.x.org
for help.
Please also check the log file at "/usr/local/XSGX/var/log/Xorg.0.log" for additional information.

Server terminated with error (1). Closing log file.

Any pointers towards these errors?

Regards,

Ketan